Does M4 run in same frequency during A9 core sleep and wakeup in imx6sx?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Does M4 run in same frequency during A9 core sleep and wakeup in imx6sx?

Jump to solution
1,239 Views
rakesh_patel
Senior Contributor I

We are using imx6sx board.

We put A9 core in sleep mode using below command.

====================

echo mem > /sys/power/state

 

Output with suspend and resume.

====================

PM: Syncing filesystems ... done.
Freezing user space processes ... (elapsed 0.001 seconds) done.
Freezing remaining freezable tasks ... (elapsed 0.001 seconds) done.
Suspending console(s) (use no_console_suspend to debug)
PM: suspend of devices complete after 137.546 msecs
PM: suspend devices took 0.140 seconds
PM: late suspend of devices complete after 0.948 msecs
PM: noirq suspend of devices complete after 0.854 msecs
Disabling non-boot CPUs ...
M4 is busy, enter WAIT mode instead of STOP!
PM: noirq resume of devices complete after 0.438 msecs
PM: early resume of devices complete after 0.529 msecs
PM: resume of devices complete after 166.078 msecs
PM: resume devices took 0.170 seconds
Restarting tasks ... done.

 

Query:

================

1) Does M4 run at same frequency during A9 suspend and wakeup ?

 

Labels (1)
0 Kudos
Reply
1 Solution
1,210 Views
igorpadykov
NXP Employee
NXP Employee

one can look at folder ../demo_apps/low_power_imx6sx

FreeRTOS_MX6SX_1.0.1_WIN

 

Best regards
igor

View solution in original post

0 Kudos
Reply
5 Replies
1,226 Views
igorpadykov
NXP Employee
NXP Employee

Hi rakesh_patel

 

I believe yes, M4 runs at the same frequency. Example for changing

M4 frequency can be found in  sect.5.1 Deep-Sleep mode

i.MX 6SoloX Power Consumption Measurement - AN5050 

 

Best regards
igor

0 Kudos
Reply
1,214 Views
rakesh_patel
Senior Contributor I

@igorpadykov :

Is there any M4 application for "Enter "S" on M4 console to change M4 to low frequency mode (12 MHz)." (Seciont#5.1 )?

 

I checked FreeRTOS_BSP_1.0.1_iMX6SX BSP. But could not find any application for the same.

 

Can you please help me here?

 

0 Kudos
Reply
1,211 Views
igorpadykov
NXP Employee
NXP Employee

one can look at folder ../demo_apps/low_power_imx6sx

FreeRTOS_MX6SX_1.0.1_WIN

 

Best regards
igor

0 Kudos
Reply
1,195 Views
rakesh_patel
Senior Contributor I

@igorpadykov :

We have custom application in M4 core running in TCM. 

In our application, we are doing GPIO reading and writing to RAM address operation from EPIT handler.

We found that, while A9 core coming back from Suspend to wakeup(from mem > sys/power/state), M4 core application speed degraded for couple of ms(2-3 ms) only. What can be the reason here? Any idea?

M4 core has an EPIT timer using "epitClockSourcePeriph" Clock. and EPIT handler doing GPIO reading and writing to RAM.

 

Any idea here? 

0 Kudos
Reply
1,237 Views
rakesh_patel
Senior Contributor I

@igorpadykov : Do you have any idea for this?

 

0 Kudos
Reply