Does IMX6 android support WIFI miracast?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Does IMX6 android support WIFI miracast?

4,706件の閲覧回数
daqiang
Contributor I

Dear Sir:

请问Freescale IMX 支持WIFI display吗?在相关资料中并没有看到显示模块有提及这部分,

还请帮忙确认。

如果支持WFD,显示部分应该有单独的模块处理显示部分的数据,暂时还未发现。

谢谢!

ラベル(4)
0 件の賞賛
返信
3 返答(返信)

3,988件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Guo

WIFI display is supported in extended feature package,

refer to sect.6 Freescale Extended Feature Packages

attached document.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

注意:如果这个职位回答你的问题,请点击正确答案按钮。谢谢!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

3,988件の閲覧回数
daqiang
Contributor I

Hi Igor:

Thanks for your answers!

How about freescale's WFD function? Does it support mirror mode and video mode?

Mirror mode: Wifi display and main LCD show the same screen

Video mode: WIFI display and main LCD can show different screen, for example,play a video.

By the way, our code base is android 4.2.2,does it still support WFD?

Thanks a lot!

Regards!

Leo Guo

0 件の賞賛
返信

3,988件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Guo

WIFI display is supported in extended feature package,

please apply to local marketing for details and additional docs.

Best regards

igor

0 件の賞賛
返信