Documentation for I.MX6 VPU Video API

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Documentation for I.MX6 VPU Video API

3,060件の閲覧回数
brainmeltdown
Contributor I

I have a copy of the i.MX VPU Application Programming Interface Linux® Reference Manual from 03/2016.  Is it current?  Is it supported.

I ask because first although the manual says

   VPU example application is located under Yocto Project build tmp work tree in imx-test/*/test/mxc_vpu_test

I can't find any such folder.  And so after much searching I found a vpu_wrapper.h file but the structures and functions in it are named differently than in the programming manual above.

I hope there is a well documented and supported API for Linux user-space program to use the VPU for H.264 encoding/decoding.

タグ(4)
0 件の賞賛
返信
1 返信

1,656件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Mike

please look at

www.nxp.com/lgfiles/NMG/MAD/YOCTO/imx-test-5.4.tar.gz

meta-fsl-arm/recipes-bsp/imx-test at master · Freescale/meta-fsl-arm · GitHub 

latest nxp linux documentation on

http://www.nxp.com/products/software-and-tools/software-development-tools/i.mx-software-and-tools/i....

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信