Documentation bugs : i.MX 6 Linux® Reference Manual, Rev. L3.14.28_1.0.0-ga, 03/2015

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Documentation bugs : i.MX 6 Linux® Reference Manual, Rev. L3.14.28_1.0.0-ga, 03/2015

1,707 次查看
rohitchandel
Contributor II

Is this doc upto date ????

I found an issue:

Page 41:

3.2.4 Interrupt Source Code Structure

The interrupt module is implemented in the following file (located in the directory

<Yocto_BuildDir>/linux/arch/arm/plat-mxc)

But there's no "plat-mxc" dir in the sources for 3.14.28, which this doc claims to be describing !!!!

Similiar references at:

Page 142

Page 165

Page 344

Page 383

Correct me if I am missing something here.

标签 (1)
3 回复数

1,475 次查看
gusarambula
NXP TechSupport
NXP TechSupport

This is indeed an error or rather a lack of update. Starting 3.10.17 there were some significant changes on the structure of the kernel source code.

As far as I know the plat-mxc files have been merged into the mach-imx directory, which is no longer located on the path mentioned on the documentation but in:

<Yocto_DIR>/<BUILD_DIR>/tmp/work-shared/<MACHINE>/kernel-source/arch/arm/mach-imx

I’ll escalate this to the documentation team so it gets addressed on the next releases of the Linux Reference Manual. Thank you for pointing these out!

1,475 次查看
nagladhana
Contributor II

Just checked Its not updated even in the latest  Document Number: IMXLXRM
Rev. 1, 01/2017.

I guess correcting this will help people better.

0 项奖励
回复

1,475 次查看
rohitchandel
Contributor II

Any timeline for update to 4.x ?

0 项奖励
回复