Display error on imx8xqxp mek

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Display error on imx8xqxp mek

862件の閲覧回数
Ale2
Contributor I

Some thing wrong happens when I play rtsp stream by gst on imx8qxp board:

1.jpg

But it works fine on imx8m board. Here is the log:

2.png

Same result when I use "rtspsrc location=rtsp://192.168.1.19:554/1/h264major latency=200 ! rtph264depay ! h264parse ! queue ! vpudec ! appsink sync=false" in my app.

Any clue about this?

Thanks,

Ale

0 件の賞賛
返信
2 返答(返信)

844件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello Ale2,

 

Make sure that both are playing the latest linux bsp, there is A53 in MX8M and A35 in MX8QX, but should not difference in display mode.

with the

gst-inspect-1.0 v4l2h264dec

you can see the difference between both processor on encoding time. Also Try the file

gst-launch-1.0 playbin uri=file:/run/media/sda1/big_buck_bunny.mp4 video-sink="imxvideoconvert_g2d ! queue ! autovideosink"

To avoid display issues.

 

 

Regards

 

0 件の賞賛
返信

837件の閲覧回数
Ale2
Contributor I

Hi,


Thanks for your reply! We expect to get data in NV12 format. In this case, we do not want to use imxvideoconvert_g2d to do further processing.

We write codes in Qt like:

VideoCapture cap;
cap.open( "rtspsrc location=rtsp://admin:admin@192.168.1.42:554/1/0.sdp ! rtph264depay ! h264parse ! queue ! vpudec! queue ! appsink sync=false", CAP_GSTREAMER)

It works well in imx8m. Then we want to port the app to imx8x. We modify the code to this:

VideoCapture cap;
cap.open( "rtspsrc location=rtsp://admin:admin@192.168.1.42:554/1/0.sdp ! rtph264depay ! h264parse ! queue ! v4l2h264dec ! queue ! appsink sync=false", CAP_GSTREAMER)

And the display error occurs in imx8x.

In IMX8GStreamerGuide.pdf, It is ok to parse rtspsrc without imxvideoconvert_g2d. Is there something we should do in this process?3.png

0 件の賞賛
返信