Display error on imx8xqxp mek

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Display error on imx8xqxp mek

1,205 Views
Ale2
Contributor I

Some thing wrong happens when I play rtsp stream by gst on imx8qxp board:

1.jpg

But it works fine on imx8m board. Here is the log:

2.png

Same result when I use "rtspsrc location=rtsp://192.168.1.19:554/1/h264major latency=200 ! rtph264depay ! h264parse ! queue ! vpudec ! appsink sync=false" in my app.

Any clue about this?

Thanks,

Ale

0 Kudos
Reply
2 Replies

1,187 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello Ale2,

 

Make sure that both are playing the latest linux bsp, there is A53 in MX8M and A35 in MX8QX, but should not difference in display mode.

with the

gst-inspect-1.0 v4l2h264dec

you can see the difference between both processor on encoding time. Also Try the file

gst-launch-1.0 playbin uri=file:/run/media/sda1/big_buck_bunny.mp4 video-sink="imxvideoconvert_g2d ! queue ! autovideosink"

To avoid display issues.

 

 

Regards

 

0 Kudos
Reply

1,180 Views
Ale2
Contributor I

Hi,


Thanks for your reply! We expect to get data in NV12 format. In this case, we do not want to use imxvideoconvert_g2d to do further processing.

We write codes in Qt like:

VideoCapture cap;
cap.open( "rtspsrc location=rtsp://admin:admin@192.168.1.42:554/1/0.sdp ! rtph264depay ! h264parse ! queue ! vpudec! queue ! appsink sync=false", CAP_GSTREAMER)

It works well in imx8m. Then we want to port the app to imx8x. We modify the code to this:

VideoCapture cap;
cap.open( "rtspsrc location=rtsp://admin:admin@192.168.1.42:554/1/0.sdp ! rtph264depay ! h264parse ! queue ! v4l2h264dec ! queue ! appsink sync=false", CAP_GSTREAMER)

And the display error occurs in imx8x.

In IMX8GStreamerGuide.pdf, It is ok to parse rtspsrc without imxvideoconvert_g2d. Is there something we should do in this process?3.png

0 Kudos
Reply