Difference between MCIMX6 and PCIMX6

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Difference between MCIMX6 and PCIMX6

ソリューションへジャンプ
2,481件の閲覧回数
danielbujak
Contributor III

I've been developing on the MX6UL EVK with the PCIMX6G2CVM05AA, but am now looking to port to a custom PCB with the MCIMX6G2AVM07AA part on it. Where can I find information on the differences between these parts that I need to be aware of for the port?

ラベル(1)
0 件の賞賛
返信
1 解決策
2,254件の閲覧回数
gusarambula
NXP TechSupport
NXP TechSupport

Hello Danielbujak,

The PC in front of the par number refers to the part being a prototype sample. You can see more details on what the part number nomenclature means in figure 1 of the i.MX6UL Datahseet (link below):

http://www.nxp.com/docs/en/data-sheet/IMX6ULCEC.pdf

I hope this helps!

Regards,

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,255件の閲覧回数
gusarambula
NXP TechSupport
NXP TechSupport

Hello Danielbujak,

The PC in front of the par number refers to the part being a prototype sample. You can see more details on what the part number nomenclature means in figure 1 of the i.MX6UL Datahseet (link below):

http://www.nxp.com/docs/en/data-sheet/IMX6ULCEC.pdf

I hope this helps!

Regards,

0 件の賞賛
返信
1,751件の閲覧回数
brian_21
Contributor I

For Special Qualification level, is the SC marked at the package body for this type of device?

0 件の賞賛
返信