Designing a schematic for NXP imx6ull MCIMX6Y2DVM09AB

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Designing a schematic for NXP imx6ull MCIMX6Y2DVM09AB

10,254 Views
Nikunj_Solanki
Contributor III

Hi everyone,

I'm designing a schematic based on the NXP imx6ull MCIMX6Y2DVM09AB processor and I'm looking for some help from the NXP community.

Specifically, I'm interested in the following areas:

  1. Power supply scheme: How many different voltages are required for the imx6ull MCIMX6Y2DVM09AB processor? What are the typical voltage levels and current requirements for each voltage?
  2. Power supply sequence: What is the recommended power supply sequence for the imx6ull MCIMX6Y2DVM09AB processor? Are there any specific timing requirements or considerations?
  3. Component selection: How do I select the right components for the power supply section? What are the key factors, such as voltage regulators, capacitors, and inductors?
  4. Schematic design guidelines: Are there any specific guidelines or best practices for designing a schematic for the imx6ull MCIMX6Y2DVM09AB processor?

I would greatly appreciate any advice or insights you can provide. I appreciate any help you can provide.

Best regards,

Tags (2)
0 Kudos
Reply
15 Replies

10,197 Views
Nikunj_Solanki
Contributor III

Can you please verify the PMIC Parts number?
MC32PF1550A0EP

0 Kudos
Reply

10,176 Views
Rita_Wang
NXP TechSupport
NXP TechSupport
0 Kudos
Reply

10,172 Views
Nikunj_Solanki
Contributor III

Thank You so much for your support!

10,198 Views
Nikunj_Solanki
Contributor III

Thank You so much for your response.
I am using DDR3L SDRAM so, any special power supply required to manage DDR3L in the NXP datasheet mentioned is 1.35V.

0 Kudos
Reply

10,178 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Yes, for DDR3L the power is 1.35, You can use the DDR3L on the i.MX6ULL just following the Hardware Development Guide for the i.MX 6ULL Applications Processor.

0 Kudos
Reply

10,228 Views
Nikunj_Solanki
Contributor III

Yes, I want to choose to use PMIC, Please suggest.

0 Kudos
Reply

10,232 Views
Nikunj_Solanki
Contributor III

Yes, I want to choose PMIC, so please recommend and can you please explain to me a power on/off sequence?

0 Kudos
Reply

10,204 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Details you can see in our datasheet:

Rita_Wang_0-1729738996362.png

For the design with PMIC, I email to you.

10,169 Views
Nikunj_Solanki
Contributor III

I am using DDR3L and am a little bit confused about the VDD_SOC_IN voltage configuration. According to a datasheet, its range is from 1.15V to 1.3V. So, which voltage is suitable for my application?

0 Kudos
Reply

10,138 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

PMIC can out put what the voltage you want for the VDD_ARM_SOC_IN, so you do not care about it, if you choose the PMIC in your design.

0 Kudos
Reply

10,135 Views
Nikunj_Solanki
Contributor III

But, I don't know exactly which voltage is chosen for VDD_SOC_IN.

Does it affect DDR3L if I choose 1.05V or 1.225V?

0 Kudos
Reply

9,980 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

For the VDD_SOC_IN it need 1.275 to 1.5 for 528MHz for A7 core work, and  1.375 to 1.5 for 900MHz for A7 core work.

Rita_Wang_0-1730181519830.png

From the design I share to you, you can see that for the VDD_SOC_IN it is supply from the SW1 of the PF1550.

Rita_Wang_0-1730189285660.png

Rita_Wang_1-1730189349782.png

From the PF1550 datasheet you can see that the SW1 can supply:

SW1, 1.0 A; 0.6 V to 1.3875 V in 12.5 mV steps, or 1.1 V to 3.3 V in variable steps

So it can supply what the VDD_SOC_IN need, so you do not know what the exactly the value it is.

PMIC with 1A Li+ Linear Battery Charger | NXP Semiconductors

PF1550, Power management integrated circuit (PMIC) for low power application - Data sheet

Rita_Wang_2-1730189440591.png

 

 

For the DDR3L, the Voltage is 1.35V, and the power for the DDR is from NVCC_DRAM power, DDR will effect by it:

Rita_Wang_0-1730168312112.png

 

0 Kudos
Reply

9,975 Views
Nikunj_Solanki
Contributor III

Thank You so much for your support.

Tags (1)

10,229 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

You can refer to our reference design and hardware design guide document, and following our datasheet, following the power on/off sequnce.

Do you need to choose use PMIC IC or not?

10,212 Views
Nikunj_Solanki
Contributor III
Please share reference design file and suggest PMIC IC
0 Kudos
Reply