Default condition of SCU_WDOG_OUT pin

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Default condition of SCU_WDOG_OUT pin

跳至解决方案
1,191 次查看
Kazuma_Sasaki
Senior Contributor I

Let me confirm deafult condition of SCU_WDOG_OUT pin.

Datasheet mentioned SCU_WDOG_OUT pin is configured WDOG_OUT function and 50k PullDown.

But, reference manual mentioned SCU_WDOG_OUT pin is configured JTAG_TRST function and bus-keeper.

Which information is correct?

From IMX8DXAEC Rev. 2, 11/2019

pastedImage_1.png

From IMX8DQXPRM Rev. E, 06/2019

pastedImage_3.png

pastedImage_6.png

pastedImage_7.png

pastedImage_2.png

Best Regards,

Kazuma Sasaki.

标记 (1)
0 项奖励
回复
1 解答
1,049 次查看
joanxie
NXP TechSupport
NXP TechSupport

I got suggestion as below:

 JTAG_TRST_B function was removed, it was replaced as SCU_WDOG_OUT. Do not pull-up this pin to SCU_1V8. Suggest add one pull-down resistor on this pin.

在原帖中查看解决方案

0 项奖励
回复
3 回复数
1,049 次查看
3217768732
Contributor I

Hello ,bro,I met one problem with SCU_WDOG_OUT,when powerd up, SCU_WDOG_OUT output an waveform like below,did u ever solve this kind of things? thx a lot

0 项奖励
回复
1,050 次查看
joanxie
NXP TechSupport
NXP TechSupport

I got suggestion as below:

 JTAG_TRST_B function was removed, it was replaced as SCU_WDOG_OUT. Do not pull-up this pin to SCU_1V8. Suggest add one pull-down resistor on this pin.

0 项奖励
回复
1,049 次查看
Kazuma_Sasaki
Senior Contributor I

Dear Joan,

I appreciate your support.

I understand that the contents of datasheet are correct and reference  manual will be revised in the near future.

Best Regards,

Kazuma Sasaki.

0 项奖励
回复