Let me confirm deafult condition of SCU_WDOG_OUT pin.
Datasheet mentioned SCU_WDOG_OUT pin is configured WDOG_OUT function and 50k PullDown.
But, reference manual mentioned SCU_WDOG_OUT pin is configured JTAG_TRST function and bus-keeper.
Which information is correct?
From IMX8DXAEC Rev. 2, 11/2019
From IMX8DQXPRM Rev. E, 06/2019
Best Regards,
Kazuma Sasaki.
Solved! Go to Solution.
I got suggestion as below:
JTAG_TRST_B function was removed, it was replaced as SCU_WDOG_OUT. Do not pull-up this pin to SCU_1V8. Suggest add one pull-down resistor on this pin.
Hello ,bro,I met one problem with SCU_WDOG_OUT,when powerd up, SCU_WDOG_OUT output an waveform like below,did u ever solve this kind of things? thx a lot
I got suggestion as below:
JTAG_TRST_B function was removed, it was replaced as SCU_WDOG_OUT. Do not pull-up this pin to SCU_1V8. Suggest add one pull-down resistor on this pin.
Dear Joan,
I appreciate your support.
I understand that the contents of datasheet are correct and reference manual will be revised in the near future.
Best Regards,
Kazuma Sasaki.