Default Frequency of ACLK_EIM_SLOW_CLK_ROOT

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Default Frequency of ACLK_EIM_SLOW_CLK_ROOT

587 Views
eishishibusawa
Contributor III

Dear Sir

 

I want to confirm about the Default Frequency of ACLK_EIM_SLOW_CLK_ROOT.

 

I refer to the i.MX6DulaLite reference manual (IMX6SDLRM Rev.2) .

It is described as following.

P796 Table 18-4

ACLK_EIM_SLOW_CLK_ROOT = 198MHz

 

Q1.

I think that the default value is 132MHz.

Can I understand that this description (value) is typo?

 

Best Regards,

Eishi SHIBUSAWA

Labels (1)
0 Kudos
Reply
1 Reply

470 Views
Yuri
NXP Employee
NXP Employee

Hello

please refer to https://community.nxp.com/thread/442559 

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply