Hi, all.
I'm very newbie. Is it possibile to install debian within this processor?
If not, which processor supports it?
UPDATE
The board in issue is this: PLC operator panel, PLC with HMI
Yes, it is possible.
Here is a tutorial for mx23 that you can refer to and adapt it to mx28:
https://eewiki.net/display/linuxonarm/iMX233-OLinuXino
Regards,
Fabio Estevam
Thank you Fabio.
I updated the question with the spec of the board and maybe I've too low memory to mount debian.
However, what do you mean with 'adapt it to mx28'? Should I change something?
For example in the section Bootloader -> patches I see:
wget -c https:
//rcn-ee.com/repos/git/u-boot-patches/v2015.10-rc3/0001-mx23_olinuxino-uEnv.txt-bootz-n-fixes.patch
patch -p1 <
0001
-mx23_olinuxino-uEnv.txt-bootz-n-fixes.patch
That seems to be specific for mx23 .. isn't it?
Sure it is possible, in fact we have an UBUNTU BSP for the i.MX28EVK that you find in the following link, and since UBUNTU it is a distro from Debian, there is no limitation on the usage of Debian with any of the i.MX