Debian build fail ( tflite_ethosu_delegate] Error 2) in flexbuild v24.12 and imx8mpevk.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Debian build fail ( tflite_ethosu_delegate] Error 2) in flexbuild v24.12 and imx8mpevk.

1,994件の閲覧回数
charleshuang
Senior Contributor II

Hi NXP,

We are following the NXP Release Debian 2024/12/30 version as per the official documentation:

https://docs.nxp.com/bundle/UG10155/page/topics/building_an_image_in_flexbuild.html

We followed the standard procedure described in the "Most used examples with automated build" section and run the command:

blb -m imx8mpevk

We understand that this process may involve building a Debian Docker image with ML features.

Could you confirm whether it is possible to successfully compile the Docker image using this method?
If not, could you provide the correct SOP (Standard Operating Procedure) for building it?

We have strictly followed NXP's official SOP, but we are encountering issues.
Please let us know the correct steps to complete the build successfully.

Thanks,

 

 

build_fail.jpg

0 件の賞賛
返信
6 返答(返信)

1,978件の閲覧回数
Zhiming_Liu
NXP TechSupport
NXP TechSupport
0 件の賞賛
返信

1,959件の閲覧回数
charleshuang
Senior Contributor II

Hi @Zhiming_Liu 

In the thread, you say : "Please use Ubunut22.04 as host environment."

So, do you mean we shouldn't use the Docker environment?

Please provide the correct the SOP.  Thanks.

0 件の賞賛
返信

1,953件の閲覧回数
Zhiming_Liu
NXP TechSupport
NXP TechSupport

Hello,

If you need ML feature, you need use docker under Ubuntu22.04.

Ubuntu22.04----->without ML

Ubuntu22.04+Debian12 docker------>ML/non-ML

Best Regards,
Zhiming

0 件の賞賛
返信

1,927件の閲覧回数
charleshuang
Senior Contributor II

Hi @Zhiming_Liu 

We tested on two different Ubuntu 22.04 PCs, both using the Debian 12 Docker image provided by NXP.

However, the compilation still failed.

Do you have any suggestions?"

0 件の賞賛
返信

1,891件の閲覧回数
charleshuang
Senior Contributor II

Hi @Zhiming_Liu 

Thanks for your help.

We change use the Azure VM (Cloud vm), the result is pass.

タグ(1)
0 件の賞賛
返信

1,955件の閲覧回数
charleshuang
Senior Contributor II

Hi @Zhiming_Liu 

May I compile without ML?
Do you have any advice?

Thanks.

タグ(1)
0 件の賞賛
返信