De-interlace Capture Device issue

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

De-interlace Capture Device issue

2,368 Views
m_c
Senior Contributor I

Add apply patch at <De-interlace Capture Device>, the image became blur. Is this right? How to improve it?

01_original = Freescale Android JB4.3 1.1.0

14132_14132.png03_original_zoom.png

02_deinterlace.png

After apply deinterlance patch

14134_14134.png04_deinterlace_zoom.png

Labels (3)
0 Kudos
Reply
3 Replies

2,011 Views
rotechen
Contributor I

I have same issue with m.c. I using "Freescale Android JB4.3 1.1.0" with iMX6DL.

If I don't add the patch, the image will some interlacing artifacts in edge of motion object. It show as below.

CSI_MEM_side_effect.png

 

If i adding apply patch at <De-interlace Capture Device>, the image became blur. How to improve it?

0 Kudos
Reply

2,011 Views
SergioSolis
NXP Employee
NXP Employee

That patch is rather old for JB4.3, it shouldn't be necessary

Are you able to see the images sharp without the patch? ( I see that the image you posted is at 500% zoom so i cannot determine it)

2,011 Views
m_c
Senior Contributor I

Without patch

01_original.png

With patch

02_deinterlace.png

0 Kudos
Reply