DRIVER FOR OV5640 CAMERA

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

DRIVER FOR OV5640 CAMERA

4,441 次查看
sivakumarganesa
Contributor III

Hi all,

In our design we are using OV5640 camera module chip with sololite processor. if any driver is available for OV5640  through online please let me know.

Thanks,

Sivakumar

标签 (2)
3 回复数

3,327 次查看
SergioSolis
NXP Employee
NXP Employee

Hello Sivakumar,

Our sabre sdp board uses the OV5640 camera, you can find the driver in the following path:

kernel_imx/drivers/media/video/mxc/capture/


Have a great day,
Sergio

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

3,327 次查看
bensarusi
Contributor I

Hello Sergio,

The OV5640 camera sensor also support jpeg output format.

All the available driver I found on the net, support only YUV output format.

What are the steps i need to do, at the ov5640 driver, to make it work?

I use i.MX 6SoloLite with parallel output interface.

Thanks,

Ben

0 项奖励
回复

3,327 次查看
saurabh206
Senior Contributor III

Hi

Sivakumar

OV5640 driver is available in Freescale Linux kernel.

Thanks

Saurabh

0 项奖励
回复