DRDY polarity

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
962件の閲覧回数
wushengyong
Contributor II

The TFT uses DRDY signal, no HSYNC and VSYNC. The polarity of DRDY of TFT requires high active, but in iMX DS, it is active low, could the polarity to be set to high? the same question for CLK.

ラベル(2)
1 解決策
860件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

  It is possible change the polarity of the IPU output. Please refer to IPUx_DI0_POL register

description in I.MX6 RM. Note, for i.MX6, signal IPUx_DIx_PIN15 is used DRDY/DV (Data
validation/blank, data enable
).


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

2 返答(返信)
860件の閲覧回数
wushengyong
Contributor II

Got it, thanks!

0 件の賞賛
返信
861件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

  It is possible change the polarity of the IPU output. Please refer to IPUx_DI0_POL register

description in I.MX6 RM. Note, for i.MX6, signal IPUx_DIx_PIN15 is used DRDY/DV (Data
validation/blank, data enable
).


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------