DRAM Initialization problem in u-boot on android Prebuilt-Image for SCM i.MX6Q 1GB QWKS REVC board

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

DRAM Initialization problem in u-boot on android Prebuilt-Image for SCM i.MX6Q 1GB QWKS REVC board

5,529 Views
manojsampathkum
Contributor II

Hi,

I am using SCM i.MX6Q 1GB QWKS REVC board . I tried to boot the board with the Prebuilt-images of android. (images_M6.0.1_2.1.0-ga_MX6SCM).

I partitioned the sd card using fsl-sdcard-partition.sh and placed the images in sd card as instructed in the manual.

But when i tried to boot the board i am facing DRAM Initialization problem in uboot level

U-Boot 2015.04-00008-gcac6ef2 (May 05 2017 - 17:00:08)

CPU: Freescale i.MX6Q rev1.5 at 792 MHz
CPU: Temperature 37 C
Reset cause: POR
Board: MX6DQSCM-QWKS-REV3
I2C: ready
DRAM:

After this the board hangs. Is there any lastest prebuilt images or how to fix this issue.

Thanks,

Manoj

Labels (2)
Tags (2)
10 Replies

4,871 Views
igorpadykov
NXP Employee
NXP Employee

Hi Manoj

for programming sd please try to use mfg tool from link

https://www.nxp.com/webapp/Download?colCode=SCM-i.MX6-MFGTOOLS-LIN&appType=license&Parent_nodeId=145... 

Images can be found on
https://www.nxp.com/products/single-chip-modules/single-chip-module-i.mx-6q:SCM-i.MX6Q?tab=Design_To...

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

4,871 Views
manojsampathkum
Contributor II

Hi Igor,

I tried with the mfgtool and prebuilt-images as you guided but still same problem persists .

The board hangs in same level.

Is there any other fix for this issue??

Thanks,

Manoj

0 Kudos
Reply

4,871 Views
igorpadykov
NXP Employee
NXP Employee

Hi Manoj

sorry I am not aware of other prebuilt-images.

Best regards
igor

0 Kudos
Reply

4,871 Views
manojsampathkum
Contributor II

Hi Igor , 

I'm  using the same images which you posted above 

https://www.nxp.com/products/single-chip-modules/single-chip-module-i.mx-6q:SCM-i.MX6Q?tab=Design_To...

But I am not able to boot the board with the images which you've provided .

Hoping for a best fix Igor 

Thanks ,

Manoj.

0 Kudos
Reply

4,871 Views
igorpadykov
NXP Employee
NXP Employee

Hi Manoj

seems it is working as for example on below thread:

Watchdog reboot on overloading GPU in SCM IMX6Q 

Best regards
igor

0 Kudos
Reply

4,871 Views
manojsampathkum
Contributor II

Hi Igor

In this thread  Watchdog reboot on overloading GPU in SCM IMX6Q they are discussing about Linux imx-4.1.15-2.0.0_ga release and Yocto krogoth build.

Linux Images are working fine . But i have raised the query for for ANDROID Marshmallow images  SCM_IMX6_M6.0.1_2.1.0_ANDROID_DEMO_BSP  which are not working properly.

Hope things are clear Igor.

Looking forward for a best fix.

Regards

Manoj

0 Kudos
Reply

4,871 Views
igorpadykov
NXP Employee
NXP Employee

Hi Manoj

mentioned package "Binary Demo Files of Android M6.0.1_2.1.0 BSP - QWKS Board

for SCM-i.MX 6DQ and EVB for SCM-i.MX 6SoloX" has binaries for i.MX6SX and i.MX6DQ,

recheck that correct image for i.MX6Q (REVC (rev3) board) was used. Please use Android

User's Guide Chapter 4 Run Android with Prebuilt Image
https://www.nxp.com/docs/en/user-guide/SCMIMX6AUG.pdf

Best regards
igor

0 Kudos
Reply

4,871 Views
manojsampathkum
Contributor II

Hi Igor

I rechecked the package  I am using the images which are under qwks_rev3 directory and was doing all things as explained in Android User guide for SCM https://www.nxp.com/docs/en/user-guide/SCMIMX6AUG.pdf

Then what is our next move ??

Best regards ,

Manoj

0 Kudos
Reply

4,871 Views
igorpadykov
NXP Employee
NXP Employee

Hi Manoj

 

suggest to build image from sources.

 

Best regards
igor

0 Kudos
Reply

4,871 Views
manojsampathkum
Contributor II

Hi Igor

I built the images from the source  

I referred this manual  https://www.nxp.com/docs/en/user-guide/SCMIMX6AUG.pdf to build images.

After that, I tried to boot with newly built images but the same problem occurs.

the board hangs in the same level as I have posted earlier.

Any solution for this Igor?

best regards

Manoj

0 Kudos
Reply