DP83867 ethernet phy support for IMX8MP

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

DP83867 ethernet phy support for IMX8MP

1,730 Views
Ben10
Contributor II

We are a working on developing Windows IOT support for a custom board based on IMX8MPlus. We are using DP83867 ethernet phy instead of RTL8211F ethernet phy which was used in the IMX8MPlus board.

We have changed the phy addrress w.r.t DP83867 but the internet is not working in windows IOT. But it is working on linux. So are there any changes that needs to be done?? IMX8MPLUS 

0 Kudos
Reply
1 Reply

1,711 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

For linux side you don't have to do anything since it is supported, but for Windows side you must create the driver and compile the whole wince BSP, if you need help on this have to send a email to your microsoft account.

Regards

 

0 Kudos
Reply