DMIC input volume very low

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

DMIC input volume very low

1,818件の閲覧回数
anushan
Contributor III

Hello Everyone,

I am trying to record voice through the dmic present on my board, the audio codec used is wm8962, the codec provides 1.8v to the dmic and dmic clock runs at 2.8MHz. But, when I record anything through the dmic i am not able to hear anything in the playback.

Kindly help to find a solution.

Regards,

Anusha

0 件の賞賛
返信
1 返信

1,762件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Anusha

one can try to tweak "attenuation" factor described in Table 7-7. Audio Mixer controls 

Linux Manual in Linux 5.4.3_1.0.0 Documentation

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信