DDR4 CK_A and CK_B Functionality

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

DDR4 CK_A and CK_B Functionality

Jump to solution
2,426 Views
alistair_schofi
Contributor I

Hi,

I'm currently designing a module using the i.MX8MQ and I am in the middle of creating a schematic using 4 Micron DDR4 x8 memory chips. I'm slightly apprehensive about the usage of CK_T/C_A and CK_T/C_B. I was just wondering how these clocks should be connected to the 4 independent DDR4 chips? I (quite possibly naively) think that CK_A should run to bytes 0 and 1 of the DDR4 and that CK_B should run to bytes 2 and 3 because the LPDDR4 used on the reference design sort of implies that is the case. Can someone confirm this is correct for me? I've also tried to find something more explicit in the hardware design guide but have been unable to do so.

Thanks for any help in advance.

Tags (1)
1 Solution
2,273 Views
Yuri
NXP Employee
NXP Employee

Hello,

 

  CK_T/C_A  are intended for CS0 and CK_T/C_B - for CS1.

 

Have a great day,

Yuri

 

------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer

button. Thank you!

View solution in original post

3 Replies
2,274 Views
Yuri
NXP Employee
NXP Employee

Hello,

 

  CK_T/C_A  are intended for CS0 and CK_T/C_B - for CS1.

 

Have a great day,

Yuri

 

------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer

button. Thank you!

2,273 Views
alistair_schofi
Contributor I

Thanks for the help Yuri, I appreciate it.

If I could be cheeky and ask a quick follow up question...

Am I right in presuming that if I am using 4 DDR4 x8 memory chips then the first 2 devices/bytes would receive this CK_T/C_A, CS0, CKE0 and ODT0? And conversely the second 2 device/bytes would receive CK_T/C_A, CS0, CKE0 and ODT0?

Thanks again for your help in advance.

0 Kudos
Reply
2,273 Views
Yuri
NXP Employee
NXP Employee

Hello,

   Yes, You configuration is correct, assuming 32-bit data port at CS0.   

Regards,

Yuri.

0 Kudos
Reply