DDR3 routing rules - different signal velocity on inner layers

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

DDR3 routing rules - different signal velocity on inner layers

2,242 次查看
jakob_u
Contributor II

The signal velocity on internal layers is over 10% slower than it is on outer layers ( http://www.altera.com/literature/an/an224.pdf figure 9). The difference is so big that if you ignore it, you may end up actually violating the allowed length differences (as stated in the HDG) by far.

Still, the fact that the signal propagates slower on the inner layers seems to never be mentioned in the IMX6 documentation.

What's going on here? Will the error just be absorbed by the safety factors?

标签 (6)
标记 (4)
0 项奖励
回复
3 回复数

1,748 次查看
Yuri
NXP Employee
NXP Employee

  Generally it is highly recommended to provide careful PCB signals simulation to

analyze signal rise-times and trace lengths to see if we need to concern with

transmission line effects.  Corresponding simulation software includes most

significant factors. 

  The considerations of app notes / design checklists  are mainly just rules of

thumb in order to provide basis for estimations. In the same time, rules provided

there, are very difficult to satisfy, because they include some margin of safety.

1,748 次查看
jakob_u
Contributor II

Dear Yuri! Based on your answer, we are trying to get the simulation started.

However, we cannot find an IBIS model for the IMX6Q. It seems to exist as it is mentioned here https://community.freescale.com/thread/310902 .

Could you provide a link to the IMX6Q IBIS model file?

0 项奖励
回复

1,748 次查看
Yuri
NXP Employee
NXP Employee

The i.MX6 Q IBIS files should be updated soon and are not available on the Web now.

Would You please create a SR to get a preliminary version ?

(I think public community is not proper place to locate preliminary releases.) 

0 项奖励
回复