DDR3 - What are good delay windows?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

DDR3 - What are good delay windows?

1,402件の閲覧回数
tkl
Contributor II

Hi,

after using the DDR Stress Tester to get calibration values for DDR3 according to "Freescale i.MX6 Port Application Guide - DDR3" I am wondering how to judge the resulting delay windows. In the document it says on freescale evaluation boards the window for DQS gating is 1.1 to 1.2 tCK and for read write delay it is 0.3 to 0 4 tCK. So this are good, acceptable values? I have nothing to compare it to. What windows are you getting on your designs?

1 返信

1,283件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Torben

yes these margin values which gives MX6 DRAM Port Application Guide-DDR3

on p.14,17 are good and recommended

Freescale i.MX6 DRAM Port Application Guide-DDR3 

pastedImage_2.jpg

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------