DDR3 Trace Length

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

DDR3 Trace Length

1,866件の閲覧回数
Jochi119
Contributor II

Hello,

I am designing a board with the i.MX6Q and (4) 2GBIT 800MHZ FBGA modules on board.  I have read the Hardware Development Guide from Freescale regarding keeping the trace lengths as equal in length as possible.  My question though is as follows:  The guide requests that I keep my clock traces to a max length of 2.25 inches and every other trace group smaller than that.  In my design, I can't keep my Address lines smaller than 4.5 inches in length for the group.  Where can I compromise the recommendations?  Do I make my clock lines at least 4.5 inches in length, or leave the clock lines as is and the address lines would just be longer than the clock?

Thanks in advance,

Joseph

ラベル(5)
0 件の賞賛
返信
1 返信

1,697件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Joseph

in this case clock line should be increased up to 4.5 inches, so

when clock arrives all control/data were in proper place.

In general, if layout rules can not be followed, ibis modelling should be implemented

so all timings were calculated based on specific board conditions.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信