DDR3 T Branch routing

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

DDR3 T Branch routing

3,780 Views
jozef_s
Contributor I

Hello,

I have a question about routing topology of DDR3. In design I use two  DDR3s, which are connected in T branch topology. Then termination and extra Vtt regulator are not necessary. 

Should the address trace (ADDR0..ADDR15) from T branch to both memories the same length?

Thanks!

jozef

Labels (2)
0 Kudos
Reply
1 Reply

3,198 Views
gusarambula
NXP TechSupport
NXP TechSupport

Hello Jozef Szigl,

Yes, when using T topology, the address signals should be the same length for all DDR chips. There is some margin,  You don’t mention which processor you are using but for the i.MX6 for example address traces routing should match with a ± 25 mils margin.

You can find more details on recommended routing for the i.MX6 on the HW Design Guide (link below), although these are not unique to the i.MX6.

http://www.nxp.com/assets/documents/data/en/user-guides/IMX6DQ6SDLHDG.pdf

I hope this helps!

Regards,

0 Kudos
Reply