DDR3 Memory bus IMX6DL

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

DDR3 Memory bus IMX6DL

1,892件の閲覧回数
sebastien_puel
Contributor I

Hi all,

I would like to use an IMX6 Dual Lite with less than 4 DDR3 chips, so in 16 or 32 bit DDR3 mode

Somebody can tell if this is possible ?

Thanks.

ラベル(1)
タグ(1)
0 件の賞賛
返信
3 返答(返信)

1,768件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Sébastien

yes this is possible

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

1,768件の閲覧回数
sebastien_puel
Contributor I

Thanks for this answer.

Have you any datasheet or application note for bus use in 16 or 32 bit ? 

I find documentation only for 1x64 bit (DDR3) or 2x32 bit (LP-DDR2).

Regards,

Sébastien

0 件の賞賛
返信

1,768件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

size is defined by MMDCx_MDCTL[DSIZ] DDR data bus size. Also one can check presentation on

DES-N1936 i.MX 6UltraLite DDR Tools Overview and Hardware Design Considerations.pdf 

Best regards
igor

0 件の賞賛
返信