DDR3 Bit Swaaping

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

DDR3 Bit Swaaping

跳至解决方案
1,378 次查看
muralikrishna
Contributor I

We swapped the DDR3 bits as recommended.

How to map these bits to processor while initializing.

标签 (1)
标记 (4)
0 项奖励
回复
1 解答
1,195 次查看
CommunityBot
Community Manager
This an automatic process.

We are marking this post as solved, due to the either low activity or any reply marked as correct.

If you have additional questions, please create a new post and reference to this closed post.

NXP Community!

在原帖中查看解决方案

0 项奖励
回复
5 回复数
1,196 次查看
CommunityBot
Community Manager
This an automatic process.

We are marking this post as solved, due to the either low activity or any reply marked as correct.

If you have additional questions, please create a new post and reference to this closed post.

NXP Community!
0 项奖励
回复
1,195 次查看
art
NXP Employee
NXP Employee

Also, when swapping the byte lanes, don't forget to route correctly the strobe and mask signals, i.e. DQMx, DQSx and DQSx_B, corresponding to these byte lanes.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复
1,195 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Murali

there is no need for additional mapping or software reconfiguration, as

it is done automatically. Bit swapping is described in sect.3.5.1 Swapping data lines IMX6DQ6SDLHDG also

below part of p.4 SPF-27392 Sabre Schematic i.MX6_SABRE_SDP_DESIGNFILES :

SPF-27392   p.4.jpg

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复
1,195 次查看
muralikrishna
Contributor I

Hi igor,

Bit swapping in Hardware is taken care.

How to implement those bit swappings in software to write or read to DDR3

Murali

0 项奖励
回复
1,195 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Murali

in general it is not possible to implement bit swappings in software.

If you followed Freescale recommmendations, there is no need

for additional mapping or software reconfiguration,

Best regards

igor

0 项奖励
回复