DDR stressTest imx8mp LPDDR4

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

DDR stressTest imx8mp LPDDR4

7,295件の閲覧回数
Cyriactoms
Contributor III

I am running a ddr test for imx8mp lpddr4

I am using   MT53E1G32D2FW-046 WT:A   lpddr4/sdram  

For running the ddr tool i have created .ds file will attach the file here 

While downloading the script for calibration its showing like

Download is complete
Waiting for the target board boot...

===================hardware_init=====================


********Found PMIC PCA9450**********
hardware_init exit

*************************************************************************

*************************************************************************

*************************************************************************
MX8 DDR Stress Test V3.30
Built on Nov 24 2021 13:52:12
*************************************************************************

Waiting for board configuration from PC-end...

--Set up the MMU and enable I and D cache--
- This is the Cortex-A53 core
- Check if I cache is enabled
- Enabling I cache since it was disabled
- Push base address of TTB to TTBR0_EL3
- Config TCR_EL3
- Config MAIR_EL3
- Enable MMU
- Data Cache has been enabled
- Check system memory register, only for debug

- VMCR Check:
- ttbr0_el3: 0x97d000
- tcr_el3: 0x2051c
- mair_el3: 0x774400
- sctlr_el3: 0xc01815
- id_aa64mmfr0_el1: 0x1122

- MMU and cache setup complete

*************************************************************************
ARM clock(CA53) rate: 1800MHz
DDR Clock: 2000MHz

============================================
DDR configuration
DDR type is LPDDR4
Data width: 32, bank num: 8
Row size: 17, col size: 10
Two chip selects are used
Number of DDR controllers used on the SoC: 1
Density per chip select: 4096MB
Density per controller is: 8192MB
Total density detected on the board is: 8192MB
============================================


Please re-download with the correct value

i am not able to calibrate. Is the issue regarding the imx8mplpddr4 spreadsheet or any other issues. 

タグ(1)
0 件の賞賛
返信
9 返答(返信)

7,259件の閲覧回数
Cyriactoms
Contributor III

In the ddr controller spreadsheet i have given the value 

Density per channel per chip select (Gb)1:8
Number of Channels2
Number of Chip Selects used22
Total DRAM density (Gb)32

 

when running the stress test the out put showing 

DDR configuration
DDR type is LPDDR4
Data width: 32, bank num: 8
Row size: 17, col size: 10
Two chip selects are used
Number of DDR controllers used on the SoC: 1
Density per chip select: 4096MB
Density per controller is: 8192MB
Total density detected on the board is: 8192MB

 

which is not same as in the spreadsheet

 

 

0 件の賞賛
返信

7,236件の閲覧回数
JorgeCas
NXP TechSupport
NXP TechSupport

Hello,

Could you please try with DDR Tool for i.MX?

Also, please share your RPA file.

Best regards.

0 件の賞賛
返信

7,213件の閲覧回数
Cyriactoms
Contributor III
i am trying with ddr tool for imx and getting this output
0 件の賞賛
返信

7,212件の閲覧回数
Cyriactoms
Contributor III
 
0 件の賞賛
返信

7,189件の閲覧回数
Cyriactoms
Contributor III
DDR configuration DDR type is LPDDR4 Data width: 32, bank num: 8 Row size: 17, col size: 10 One chip select is used Number of DDR controllers used on the SoC: 1 Density per chip select: 4096MB Density per controller is: 4096MB Total density detected on the board is: 4096MB ============================================ MX8M-plus: Cortex-A53 is found ************************************************************************* ============ Step 1: DDRPHY Training... ============ ---DDR 1D-Training @1600Mhz... my calibration is not happening its getting stuck
0 件の賞賛
返信

7,181件の閲覧回数
Cyriactoms
Contributor III
INFO test_app [INFO]: Execute Training Firmware for 1D pstate0@1300MHz...
INFO test_app [INFO]: Training Firmware completed for 1D pstate0@1300MHz with status 3; Execution ended in 0s.5ms.842us...
INFO memtool.common.base_test Read phy status DDR PHY: 1D training failed
INFO root Number of logged items 0x3
ERROR memtool.common.base_test DDR PHY: 1D training failed
0 件の賞賛
返信

7,161件の閲覧回数
JorgeCas
NXP TechSupport
NXP TechSupport

Hello,

Got it, thank you for the information.

Please share the entire log with first configuration and your LPDDR4 schematic section.

Best regards.

0 件の賞賛
返信

7,110件の閲覧回数
Cyriactoms
Contributor III
It was a hardware issue it got resolved thank you
0 件の賞賛
返信

6,082件の閲覧回数
lxhan92
Contributor I

Hello, may I know the root cause of that? I have the same issue when trying to train LPDDR4 the first time.

0 件の賞賛
返信