I am running a ddr test for imx8mp lpddr4
I am using MT53E1G32D2FW-046 WT:A lpddr4/sdram
For running the ddr tool i have created .ds file will attach the file here
While downloading the script for calibration its showing like
Download is complete
Waiting for the target board boot...
===================hardware_init=====================
********Found PMIC PCA9450**********
hardware_init exit
*************************************************************************
*************************************************************************
*************************************************************************
MX8 DDR Stress Test V3.30
Built on Nov 24 2021 13:52:12
*************************************************************************
Waiting for board configuration from PC-end...
--Set up the MMU and enable I and D cache--
- This is the Cortex-A53 core
- Check if I cache is enabled
- Enabling I cache since it was disabled
- Push base address of TTB to TTBR0_EL3
- Config TCR_EL3
- Config MAIR_EL3
- Enable MMU
- Data Cache has been enabled
- Check system memory register, only for debug
- VMCR Check:
- ttbr0_el3: 0x97d000
- tcr_el3: 0x2051c
- mair_el3: 0x774400
- sctlr_el3: 0xc01815
- id_aa64mmfr0_el1: 0x1122
- MMU and cache setup complete
*************************************************************************
ARM clock(CA53) rate: 1800MHz
DDR Clock: 2000MHz
============================================
DDR configuration
DDR type is LPDDR4
Data width: 32, bank num: 8
Row size: 17, col size: 10
Two chip selects are used
Number of DDR controllers used on the SoC: 1
Density per chip select: 4096MB
Density per controller is: 8192MB
Total density detected on the board is: 8192MB
============================================
Please re-download with the correct value
i am not able to calibrate. Is the issue regarding the imx8mplpddr4 spreadsheet or any other issues.
In the ddr controller spreadsheet i have given the value
Density per channel per chip select (Gb)1: | 8 |
Number of Channels | 2 |
Number of Chip Selects used2 | 2 |
Total DRAM density (Gb) | 32 |
when running the stress test the out put showing
DDR configuration
DDR type is LPDDR4
Data width: 32, bank num: 8
Row size: 17, col size: 10
Two chip selects are used
Number of DDR controllers used on the SoC: 1
Density per chip select: 4096MB
Density per controller is: 8192MB
Total density detected on the board is: 8192MB
which is not same as in the spreadsheet
Hello,
Could you please try with DDR Tool for i.MX?
Also, please share your RPA file.
Best regards.
Hello,
Got it, thank you for the information.
Please share the entire log with first configuration and your LPDDR4 schematic section.
Best regards.
Hello, may I know the root cause of that? I have the same issue when trying to train LPDDR4 the first time.