DDR differential clock termination design rules

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

DDR differential clock termination design rules

1,442件の閲覧回数
ko-hey
Senior Contributor II

Hi all

I have a question about differential clock termination design rules.

According to the DDR section of schematics tab in following Check List,  user have to check Micron's Technical Note.

https://community.freescale.com/docs/DOC-93819

I have a question about it.

I think that user need to check only "DDR Devices's Clock Signals" section P12 and P13.

Is it correct ?

Ko-hey

ラベル(1)
0 件の賞賛
返信
1 返信

1,307件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Ko-hey

right, user needs to check "DDR Devices's Clock Signals" section P12 and P13.

Note that this app note is given as additional recommendation, so FSL documents

HW Design Checking List for i.Mx6DQSDL and IMX6DQ6SDLHDG

supersede any recommendations in that document.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信