DDR Stress Tester Option2(JTAG) for i.MX7D-Sabre didn't work

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

DDR Stress Tester Option2(JTAG) for i.MX7D-Sabre didn't work

3,255 Views
torus1000
Contributor V

Hi

I tried Option 3&2 of DDR3 stress tester with i.MX7D-Sabre.

Option 3(U-Boot) worked correctly but Option 2(JTAG) didn't display anything, I don't know why.

i.MX6/7 DDR Stress Test Tool V3.00
   https://community.nxp.com/docs/DOC-105652
i.MX7D DRAM Register Programming Aid
   https://community.nxp.com/docs/DOC-152468
      Option 3 U-Boot: ddr-test-uboot-jtag-mx7d.bin
      Option 2 DDR Stress Tester: JTAG Interface ddr-test-uboot-jtag-mx7d.elf

Here is my commands of SEGGER J-Link Jtag.

What was wrong with my setting or commands?

C:\Program Files (x86)\SEGGER\JLink_V630j>JLink.exe -device MCIMX7D7_A7_0 -CommandFile C:\jtag_init_jlink.txt
...
...
Writing 33FFFFFF -> 30000000

Writing 10000000 -> 30389800

Writing 10000001 -> 30389880
....
....
Writing 00000000 -> 30384130

Writing 00000178 -> 30340020

Writing 00000002 -> 30384130

Script processing completed.

Type "connect" to establish a target connection, '?' for help
J-Link>mem 30330120,10 /* IOMUX GPIO->UART */
30330120 = 05 00 00 00 05 00 00 00 00 00 00 00 05 00 00 00
J-Link>mem 30890080,1 /* UART1 enable */
30890080 = 01
J-Link>mem 30384940, 1 /* CCM clock gate */
30384940 = 02
J-Link>loadbin C:\Users\160703\Desktop\mx7d_ddr_cal_jtag\ddr-test-uboot-jtag-mx7d.bin 910000
Halting CPU for downloading file.
Downloading file [C:\Users\160703\Desktop\mx7d_ddr_cal_jtag\ddr-test-uboot-jtag-mx7d.bin]...
O.K.
J-Link>setpc 910000             /* Option2 image */
J-Link>g                                  /* display no characters on debug port(uart1) */
J-Link>
J-Link>
J-Link>loadfile C:\Users\160703\Desktop\mx7d_ddr_cal_jtag\ddr-test-uboot-jtag-mx7d.hex 910000
Downloading file [C:\Users\160703\Desktop\mx7d_ddr_cal_jtag\ddr-test-uboot-jtag-mx7d.hex]...
O.K.
J-Link>SetPC 910000             /* converted Option3 image */
J-Link>g                                  /* display no characters on debug port(uart1) */
J-Link>

Can anyone help me?

BTW elf file converted to ihex on the imx7d-sabre linux as following.
$ cp /run/media/mmcblk0p1/ddr*.elf .
$ objcopy -O ihex ddr-test-uboot-jtag-mx7d.elf /run/media/mmcblk0p1/ddr-test-uboot-jtag-mx7d.hex

Labels (1)
3 Replies

2,976 Views
Yuri
NXP Employee
NXP Employee

Hello,

 I.MX7 should be in serial (USB) downloader mode for JTAG.

"Normally, in order to avoid any boot media that might be present, the boot configuration is changed to serial/USB.

The device comes out of reset and ends up staying in the boot ROM as long as no valid serial boot image is fed.

The same would be true of any other boot configuration that has no valid images present. Then, JTAG can be used

from there."

  Also, the following may be helpful:

DES-N2059 ARM Development Solutions for Heterogeneous Systems 

Regards,

Yuri.

0 Kudos
Reply

2,976 Views
torus1000
Contributor V

I found my mistakes as following;

(1) init command file

removed 1st line of jtag_init_jlink.txt

//w4 30000000 33FFFFFF

(2) iomux setting

added IOMUX ALT=0 setting for RXD&TXD pin

w4 30330128 0
w4 3033012c 0

(3) uart1 enable

corrected UART2 to UART1

//w4 30890080 1
w4 30860080 1

After fixing them, it worked.

2,976 Views
torus1000
Contributor V

In my case, reset was needed before setpc command as following.

J-Link>r 
Reset delay: 0 ms
Reset type NORMAL: Toggle reset pin and halt CPU core.
J-Link>setpc 910000
J-Link>g