DDR Stress Test Tool--2.80 version

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

DDR Stress Test Tool--2.80 version

1,493 次查看
llliu
Contributor I

Hi,

      I use NXP DDR Test Tool to test MX7D.The TARGET has been choosed MX7D,and the usb has been conneted to the computer .But when I clicked Download,the result ERROR: Can't open USB device!!!

标签 (2)
标记 (1)
0 项奖励
回复
1 回复

1,298 次查看
art
NXP Employee
NXP Employee

The issue may occur if the DDR Stress Test software runs with no Administrator rights. So, please try to explicitly start the software with the Administrator rights.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复