DC spec of clock of the iMX6.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

DC spec of clock of the iMX6.

跳至解决方案
912 次查看
tomo
Contributor II

Hi all,

I am verifying clock signal of the i.MX6DL.

My custom board is use the XTAL for main clock and RTC clock.

According to "MX_design_validation_Guide_V0.1.xlsx", there are written as test point that the XTALI pad is for main clock and the RTC_XTALO pad is for RTC clock.

Why these test point are different? (Main=input side, RTC=output side)

Best regards,

tomo

标签 (1)
0 项奖励
回复
1 解答
835 次查看
Yuri
NXP Employee
NXP Employee

Hello,

  Usually output (XTALO) is used to check clock waveforms.
The requirements regarding XTALI concerns with external oscillator using.

Please refer to Table 2-7. (Oscillator and clock recommendations) of "Hardware Development Guide for i.MX 6Quad, 6Dual, 6DualLite, 6Solo Families …”

< http://cache.freescale.com/files/32bit/doc/user_guide/IMX6DQ6SDLHDG.pdf >


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
2 回复数
836 次查看
Yuri
NXP Employee
NXP Employee

Hello,

  Usually output (XTALO) is used to check clock waveforms.
The requirements regarding XTALI concerns with external oscillator using.

Please refer to Table 2-7. (Oscillator and clock recommendations) of "Hardware Development Guide for i.MX 6Quad, 6Dual, 6DualLite, 6Solo Families …”

< http://cache.freescale.com/files/32bit/doc/user_guide/IMX6DQ6SDLHDG.pdf >


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复
835 次查看
tomo
Contributor II

Hello,

Thank you for your reply.

0 项奖励
回复