DC spec of clock of the iMX6.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

DC spec of clock of the iMX6.

Jump to solution
702 Views
tomo
Contributor II

Hi all,

I am verifying clock signal of the i.MX6DL.

My custom board is use the XTAL for main clock and RTC clock.

According to "MX_design_validation_Guide_V0.1.xlsx", there are written as test point that the XTALI pad is for main clock and the RTC_XTALO pad is for RTC clock.

Why these test point are different? (Main=input side, RTC=output side)

Best regards,

tomo

Labels (1)
0 Kudos
Reply
1 Solution
625 Views
Yuri
NXP Employee
NXP Employee

Hello,

  Usually output (XTALO) is used to check clock waveforms.
The requirements regarding XTALI concerns with external oscillator using.

Please refer to Table 2-7. (Oscillator and clock recommendations) of "Hardware Development Guide for i.MX 6Quad, 6Dual, 6DualLite, 6Solo Families …”

< http://cache.freescale.com/files/32bit/doc/user_guide/IMX6DQ6SDLHDG.pdf >


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
2 Replies
626 Views
Yuri
NXP Employee
NXP Employee

Hello,

  Usually output (XTALO) is used to check clock waveforms.
The requirements regarding XTALI concerns with external oscillator using.

Please refer to Table 2-7. (Oscillator and clock recommendations) of "Hardware Development Guide for i.MX 6Quad, 6Dual, 6DualLite, 6Solo Families …”

< http://cache.freescale.com/files/32bit/doc/user_guide/IMX6DQ6SDLHDG.pdf >


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
625 Views
tomo
Contributor II

Hello,

Thank you for your reply.

0 Kudos
Reply