DART-6UL UART2

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

DART-6UL UART2

2,152 Views
francomaurizio
Contributor I

DART-6UL with WIFI-Enabled  and  BlueTooth-Disabled:

Can anybody knows how to enable UART2 on connector pins J2-84(tx) J2-86(rx) J2-88(cts_b) J2-90(rts_b)?

Thanks

bye

Labels (1)
Tags (1)
0 Kudos
Reply
1 Reply

2,006 Views
igorpadykov
NXP Employee
NXP Employee

Hi Franco

one can look at dts examples for that board

linux-2.6-imx/imx6ul-var-dart.dtsi at imx-rel_imx_4.1.15_1.1.0_ga-var02 · varigit/linux-2.6-imx · Gi... 

dart-mx6ul: Fixed pins for conflict for CAN module and UART2 · varigit/linux-2.6-imx@0fa016d · GitHu... 


Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------