Currently working camera Modules on i.mx6UL ?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Currently working camera Modules on i.mx6UL ?

1,706件の閲覧回数
thomasgadn
Contributor II

Hello everyone,

I am working currently on my Bachelor Thesis where I am working with the i.mx6UL. I am not really familiar with this processor so I wanted to ask which camera Modules are currently working. If its possible they also should be not to hard to implement. (unfortunately I cant use any camera from the OVXXXX series.)

Thank you in advance,

kind regards,

tom 

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,653件の閲覧回数
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi Tom,

You can refer to the How to use OV5640 with i.MX 6UltraLite EVK - i.MXDev Blog . It may do help for you.
Have a great day,
Rita

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

1,653件の閲覧回数
thomasgadn
Contributor II

Hello Rita,

thank you for your fast answer. Unfortunately, I cant use any Camera module from this series. I checked the blog and they say the camera is using MIPI CSI (1 or 2?).  I thought this processor is only supporting up to 24 Bit parallel RGB ?

kind regards

0 件の賞賛
返信