Creating an extra framebuffer for imx6UL

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Creating an extra framebuffer for imx6UL

1,625件の閲覧回数
zc_tee
Contributor III

Hi all,

Is it possible to create an extra framebuffer for imx6UL. I need two framebuffers (/dev/fb0 and /dev/fb1) to be associate with the LCDIF interface of imx6UL.

Thank you.

Regards,

Tee

ラベル(3)
0 件の賞賛
返信
1 返信

1,379件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi ZC

please check linux documentation related to framebuffer

http://www.tldp.org/HOWTO/text/Framebuffer-HOWTO 

How can I add an additional framebuffer device in Linux? - Unix & Linux Stack Exchange 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信