Creating MCIMX6Q-SBD Linux SD Card in Windows

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Creating MCIMX6Q-SBD Linux SD Card in Windows

3,939件の閲覧回数
bramankp
Contributor I

I've received a MCIMX6Q-SBD board and it includes an SD card that boots this thing to Android. I'd like to board to boot to Linux. I'm running Windows. I tried using MX6Q-SABRE_AI_UBUNTU_1.1.1.exe but it complains about the included SD card not having enough space. (Windows won't mount it, obvious, since it's a Linux file system.)

Is there a tool to make this easy? I can't imagine there wouldn't be but I am too new to know where to look.

ラベル(1)
0 件の賞賛
返信
6 返答(返信)

3,562件の閲覧回数
bramankp
Contributor I

Ah, this thread finally did the trick ...

https://community.freescale.com/message/365329#365329

Need to unplug the SD card when it boots and then plug it back in after it is attached to the PC so it will be flashable.

0 件の賞賛
返信

3,562件の閲覧回数
YixingKong
Senior Contributor IV

Paul

This discussion is closed since no activity. If you still need help, please feel free to reply with an update to this discussion, or create another discussion.

Thanks,

Yixing

0 件の賞賛
返信

3,562件の閲覧回数
YixingKong
Senior Contributor IV

Paul

Had your issue got resolved? If yes, we are going to close the discussion in 3 days. If you still need help, please feel free to reply with an update to this discussion.

Thanks,

Yixing

0 件の賞賛
返信

3,562件の閲覧回数
bramankp
Contributor I

So I'm gathering there is some configuration of dip switches to tell the board to boot into "flash-able" mode or something (instead of booting from the SD card)? I've been going through all the documentation I can find without any luck telling me how to configure this thing so I can use the manufacturing tool referenced above by SerchMX. Any further pointers?

0 件の賞賛
返信

3,562件の閲覧回数
SergioSolis
NXP Employee
NXP Employee

Yes, there is a tool to flash the SD:

http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=i.MX6Q&fpsp=1&tab=Design_Tools_Tab

Under "Hardware Development Tools" >> "Programmers" >> "IMX_6DQ_MFG_TOOL"

You can also find the user guide in the following link:

https://www.freescale.com/webapp/Download?colCode=L3.0.35_4.1.0_LINUX_MMDOCS&location=null&fasp=1&WT...


Best regards,
Sergio

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

3,562件の閲覧回数
bramankp
Contributor I

That's all find and good but plugging the board into my Windows 7 PC it loads a driver and calls the device "SABRESD-MX6DQ". Launching the manufacturing tool it does not find the device to write the image to. Keeps saying "Unassigned" where the documentation says it should say something like "Hub 6--Port 3".

0 件の賞賛
返信