Create UAP0 in imx6sl evk with the Android os 4.4.3

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Create UAP0 in imx6sl evk with the Android os 4.4.3

1,024件の閲覧回数
aravinthkumarja
Senior Contributor II

In Android if it connecting to AP wlan0 act as station. If we creating hotspot wlan0 act as hostap. here no separate AP(uap0) is there. so i want to create uap0. I don't know how to do this.? If anybody have idea just tell me..?

ラベル(1)
0 件の賞賛
返信
1 返信

938件の閲覧回数
CarlosCasillas
NXP Employee
NXP Employee

Hi,

Since Android 2.2, the hotspot capability is already included by default on Android itself. So, if you want to use a specific Wi-Fi chip, it is a better option to ask to the silicon manufacturer about supporting this capability, and also for requesting the proper driver for the integration with the kernel for hardware support.

Hope this will be useful for you.

Best regards!

/Carlos

0 件の賞賛
返信