Crashed when "bitbake imx-image-full"

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Crashed when "bitbake imx-image-full"

1,944件の閲覧回数
Mihan
Contributor IV

Hi 

 

I'm trying to rebuild image using fsl-5.10 in ubuntu 20.04

But it doesn't seem to work well. I have try cleaning it (bitbake -c clean imx-image-full) many times.

Here is the log in build directory "cooker".

Let me know what file you also want.

 

Best regards

Mihan 

ラベル(1)
0 件の賞賛
返信
3 返答(返信)

1,931件の閲覧回数
Zhiming_Liu
NXP TechSupport
NXP TechSupport

Try to rm the qt-base source code and retry

0 件の賞賛
返信

1,927件の閲覧回数
Mihan
Contributor IV

Hi @Zhiming_Liu 

I find the error in the log :

mkdir: cannot create directory ‘/usr/lib/opkg’: Permission denied
dpkg: error processing package nativesdk-shadow (--configure):
installed nativesdk-shadow package post-installation script subprocess returned error exit status 1

why this part will make directory in loacl system path?

Before that , there are some warnings:

dpkg: warning: while removing nativesdk-glibc-binary-localedata-zu-za.utf-8, directory '/opt/fsl-imx-fb/5.10-gatesgarth/sysroots/x86_64-pokysdk-linux/usr/lib/locale' not empty so not removed
dpkg: warning: 'ldconfig' not found in PATH or not executable
dpkg: warning: overriding problem because --force enabled:
dpkg: warning: 1 expected program not found in PATH or not executable
Note: root's PATH should usually contain /usr/local/sbin, /usr/sbin and /sbin

0 件の賞賛
返信

1,928件の閲覧回数
Mihan
Contributor IV

Thanks @Zhiming_Liu 

 

It seems to work. I finished the image building. Now I'm make the toolchain for it.

But it returns error again.

Attached is the log file, could you please check for me again?

 

Best regards

Mihan

0 件の賞賛
返信