Couldn't automate eMMC booting using MFG tool

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Couldn't automate eMMC booting using MFG tool

1,538件の閲覧回数
bazo00
Contributor I

Hello,

I am using IMX6DL based custom board.

I am trying to boot from eMMC, and I am able to do so, but only after manually setting boot_config.

It seems like this line from MFG tool doesn't work. I can not find the reason.

<CMD state="Updater" type="push" body="$ echo 8 > /sys/block/mmcblk%mmc%/device/boot_config">enable boot partion 1 to boot</CMD>

I also tried with this lines also, since I was able to find boot_config there too. Again unsuccessfully.

<CMD state="Updater" type="push" body="$ echo 8 > /sys/devices/soc0/soc.1/2100000.aips-bus/219c000.usdhc/mmc_host/mmc0/mmc0\:0001/boot_config">enable boot partion 1 to boot</CMD>
<CMD state="Updater" type="push" body="$ echo 10 > /sys/devices/soc0/soc.1/2100000.aips-bus/219c000.usdhc/mmc_host/mmc0/mmc0\:0001/boot_bus_config">enable boot partion 1 to boot</CMD>

When I set up this manually(after starting u-boot.imx and kernel directly from RAM using MFG tool) I can see bit for boot enabling set to 1, and after repower the board, it does boots up from eMMC fine.

Do you have any idea what could be the problem with MFG tool command?

ラベル(1)
0 件の賞賛
返信
1 返信

1,343件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi

one can check if appropriate version of MFG Tools used, for example

for L4.1.15_1.1.0 should be used i.MX Series Manufacturing Toolkit for Linux 4.1.15_1.1.0 Release , e.t.c.

http://www.nxp.com/products/microcontrollers-and-processors/arm-processors/i.mx-applications-process...

What nxp reference design is based custom board, sould it be reproduced on reference board.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信