I'm making a camera system using the I.MX6solo and 1.3Megapixel image sensor. For this system ISP would not be used, because any correction and format conversion in hardware are not needed. Thus the image sensor would send its bayer raw data directly to I.MX6solo. But I wonder if the MCU could receive and save such bayer raw data. Would it be possible?
Thank you very much for the answer. But please let me ask one more question. I suppose you assumed that I'd need preview or video. But if I would just save image data to memory without any processing, streaming, would I.MX6solo do the job without issue?
Yes, the i.MX6Solo processor is capable of receiving and storing a raw Bayer image data through its CSI interface.
Have a great day,
Artur
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------