Cortex M7 GPIO toggle frequency

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Cortex M7 GPIO toggle frequency

2,166 Views
andrej_valek
Contributor V

Dear community!

I have an 8MPLUSLPD4-EVK board and wanted to control the GPIO pin inside M7 core (MIMX8ML8xxxKZ). So I took the https://github.com/nxp-mcuxpresso/mcux-sdk/  and use a led_output project as an example. I wanted to toggle GPIO pin as fast as possible. The Systemclk is running at 800MHz, but the output is toggling with freq 4MHz. I know, that the GPIO bus has to be driven lower then the syslck, but not 4MHz.

 

 

// board.h
#define BOARD_SIGNAL_LOOP_GPIO      GPIO3
#define BOARD_SIGNAL_LOOP_GPIO_PIN  21U

// pin_mux.c
void BOARD_InitPins(void) {
    IOMUXC_SetPinMux(IOMUXC_SAI5_RXD0_GPIO3_IO21, 0U);
    IOMUXC_SetPinConfig(IOMUXC_SAI5_RXD0_GPIO3_IO21,
                        IOMUXC_SW_PAD_CTL_PAD_PE(1U) |
                        IOMUXC_SW_PAD_CTL_PAD_DSE(3U) |
                        IOMUXC_SW_PAD_CTL_PAD_FSEL(1U));


    IOMUXC_SetPinMux(IOMUXC_UART4_RXD_UART4_RX, 0U);
    IOMUXC_SetPinConfig(IOMUXC_UART4_RXD_UART4_RX, 
                        IOMUXC_SW_PAD_CTL_PAD_PUE_MASK |
                        IOMUXC_SW_PAD_CTL_PAD_PE_MASK);
    IOMUXC_SetPinMux(IOMUXC_UART4_TXD_UART4_TX, 0U);
    IOMUXC_SetPinConfig(IOMUXC_UART4_TXD_UART4_TX, 
                        IOMUXC_SW_PAD_CTL_PAD_PUE_MASK |
                        IOMUXC_SW_PAD_CTL_PAD_PE_MASK);
}

// main.c
#include "fsl_debug_console.h"
#include "pin_mux.h"
#include "clock_config.h"
#include "board.h"

int main(void)
{
    gpt_config_t gptConfig;

    /* Board pin, clock, debug console init */
    /* M7 has its local cache and enabled by default,
     * need to set smart subsystems (0x28000000 ~ 0x3FFFFFFF)
     * non-cacheable before accessing this address region */
    BOARD_InitMemory();

    /* Board specific RDC settings */
    BOARD_RdcInit();

    BOARD_InitBootPins();
    BOARD_BootClockRUN();
    BOARD_InitDebugConsole();

    /* Init GPIO pins as an outputs */
    gpio_pin_config_t signal_config = {kGPIO_DigitalOutput, 0, kGPIO_NoIntmode};
    GPIO_PinInit(BOARD_SIGNAL_LOOP_GPIO, BOARD_SIGNAL_LOOP_GPIO_PIN, &signal_config);

    PRINTF("Start generating signals...\r\n");

    while (1)
    {
        GPIO_PortToggle(BOARD_SIGNAL_LOOP_GPIO, 1u << BOARD_SIGNAL_LOOP_GPIO_PIN);
    }
}

 

 

I tried multiple GPIOs, but the result is still the same.

So what's wrong here? Or the other question is, how can I verify, that the systemclk is running at 800MHz.

Thanks,
Andy

Tags (1)
0 Kudos
Reply
2 Replies

2,138 Views
Manuel_Salas
NXP TechSupport
NXP TechSupport

Hello @andrej_valek 

 

Please refer to this thread.

 

Best regards,

Salas.

0 Kudos
Reply

2,114 Views
andrej_valek
Contributor V

Thank you @Manuel_Salas ,

but this won't help me I guess.

I'm using the GPIO_PortToggle function, which reflects to

static inline void GPIO_PortToggle(GPIO_Type *base, uint32_t mask)
{
#if (defined(FSL_FEATURE_IGPIO_HAS_DR_TOGGLE) && (FSL_FEATURE_IGPIO_HAS_DR_TOGGLE == 1))
    base->DR_TOGGLE = mask;
#else
    base->DR ^= mask;
#endif /* FSL_FEATURE_IGPIO_HAS_DR_TOGGLE */
}

so I guess there is no overhead. The fact (from the previous thread), that GPIO is connected to IPG_CLK_ROOT which is running at 66.66MHz won't reflect to my behavior. The output freq on that pin is 4MHz.

On the other hand, could it be that I'm touching a wrong GPIO? Or maybe, would it be possible to test it on your side or provide me an application/code for verification?

Many thanks,
Andy

0 Kudos
Reply