Cortex-M4 Core1 is not working in IMX8QM CPU

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Cortex-M4 Core1 is not working in IMX8QM CPU

3,356件の閲覧回数
pranav_vaze
Contributor I

Hi,

We are testing M4 cores in IMX8QM with pre-build and compiled binaries, in this M4 Core0 is working without any issues.

The M4 Core1 is not working with both the pre-build and compiled binaries. We are able to access the M4 Core0 and Core1 UARTs pin as GPIO in U-boot. We are using 4.14.78-GA BSP release SCFW.

Regards,
Pranav

0 件の賞賛
返信
3 返答(返信)

2,883件の閲覧回数
pranav_vaze
Contributor I

Hi Artur,

     
   We are following same commands for creating M4 binaries for booting from u-boot and booting from ROM options.
   The M4 Core0 is booting with both the boot options (We are getting output messages in M4-Core0 UART).
   The M4 Core1 is not booting with both the boot options. 

Regards,

Pranav

0 件の賞賛
返信

2,883件の閲覧回数
art
NXP Employee
NXP Employee

How do you define that the M4 Core1 does not boot? By absence of the UART output from it? Which UART do you assign to M4 Core1?

Artur

0 件の賞賛
返信

2,882件の閲覧回数
art
NXP Employee
NXP Employee

Please refer to the attached document, especially, to its Section 4.7.6 "Running the Arm Cortex-M4 image" for the information on how to build images and run the code on the M4 core(s) on various asymmetric multicore i.MX processors, including the i.MX8QM one.

0 件の賞賛
返信