Core-image-base for imx6ulevk

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Core-image-base for imx6ulevk

Jump to solution
6,401 Views
chandraevolute
Contributor V

will the git://git.freescale.com/imx/fsl-arm-yocto-bsp.git -b imx-3.14.38-6UL_ga version support core-image-base for IMX6ULEVK board if not what are the version that support core-image-base for imx6ulevk

Labels (3)
1 Solution
5,811 Views
Yuri
NXP Employee
NXP Employee

Hello,

  Yes, minimal configuration is supported for i.MX6 UL ; Qt 5 images are only

supported for i.MX SoC with hardware graphics. They are not supported on the
i.MX 6UltraLite

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
11 Replies
5,145 Views
rajesh-d
Contributor I

can we build rootfs using (core-image-rt-sdk)as image recipe in yocto toaster for imx6ull

0 Kudos
Reply
5,811 Views
vijayaragavansr
Contributor II

Hi,

i built core-image-base and succesffully flashed onto SD Card and booted as root.

but i am unable to execute reboot,poweroff,shutdown commands.  

below my terminal log

root@melange:~# poweroff
poweroff: must be superuser.
root@melange:~# reboot
reboot: must be superuser.
root@melange:~# shutdown -r now
shutdown: warning: cannot open /var/run/shutdown.pid
shutdown: /dev/initctl: Permission denied
init: must be superuser.
root@melange:~#

am surprised that when i logged in as root i do not have have full permission? something wrong with the bitbake?

0 Kudos
Reply
5,812 Views
Yuri
NXP Employee
NXP Employee

Hello,

  Yes, minimal configuration is supported for i.MX6 UL ; Qt 5 images are only

supported for i.MX SoC with hardware graphics. They are not supported on the
i.MX 6UltraLite

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
5,811 Views
chandraevolute
Contributor V

Thank you Yuri

When I do bitbake core-image-minimal .sdcard images are not generating instead .cpio images are generating. How to build .sdcard images out of .cpio

0 Kudos
Reply
5,811 Views
Yuri
NXP Employee
NXP Employee

Hello,

  Please use  Linux 4.1.15_1.1.0

i.MX 6 Series Software and Development Tool|NXP

Regards,

Yuri.

0 Kudos
Reply
5,811 Views
chandraevolute
Contributor V

finally i have built core-image-base and the rootfs is around 72 MB. This is fine with us. I used imx-3.14.38-6UL_ga version. We are not using any GUI related stuff. Thank you Yuri

5,811 Views
evgenyerlihman
Contributor IV

Hey Chandra,

Could you please share the build configurations for building core-image-base?

Thanks,

Evgeny

0 Kudos
Reply
5,811 Views
chandraevolute
Contributor V

this is my bblayer.conf file

LCONF_VERSION = "6"

BBPATH = "${TOPDIR}"

BSPDIR := "${@os.path.abspath(os.path.dirname(d.getVar('FILE', True)) + '/../..')}"

BBFILES ?= ""

BBLAYERS = " \

  ${BSPDIR}/sources/poky/meta \

  ${BSPDIR}/sources/poky/meta-yocto \

  \

  ${BSPDIR}/sources/meta-openembedded/meta-oe \

  ${BSPDIR}/sources/meta-openembedded/meta-multimedia \

  \

  ${BSPDIR}/sources/meta-fsl-arm \

  ${BSPDIR}/sources/meta-fsl-arm-extra \

  ${BSPDIR}/sources/meta-fsl-demos \

"

##Freescale Yocto Release layer

BBLAYERS += " ${BSPDIR}/sources/meta-fsl-bsp-release/imx/meta-bsp "

BBLAYERS += " ${BSPDIR}/sources/meta-fsl-bsp-release/imx/meta-sdk "

BBLAYERS += " ${BSPDIR}/sources/meta-browser "

BBLAYERS += " ${BSPDIR}/sources/meta-openembedded/meta-gnome "

BBLAYERS += " ${BSPDIR}/sources/meta-openembedded/meta-networking "

BBLAYERS += " ${BSPDIR}/sources/meta-openembedded/meta-python "

BBLAYERS += " ${BSPDIR}/sources/meta-openembedded/meta-ruby "

BBLAYERS += " ${BSPDIR}/sources/meta-openembedded/meta-filesystems "

BBLAYERS += " ${BSPDIR}/sources/meta-qt5 "

~

~

5,811 Views
evgenyerlihman
Contributor IV

Thank you so much for the answer!

Can you please share the command lines you used as well? I am also looking to build the base version without any GUI but with all the other functionality (pingpong code for example).

And if possible the procedure you use to loading the image, SD or directly.

Thanks,

Evgeny

0 Kudos
Reply
5,811 Views
chandraevolute
Contributor V

bitbake core-image-base is the command that I gave. I am using  imx-3.14.38-6UL_ga bsp version. I am using SD card.

Thanks

chandra

5,811 Views
evgenyerlihman
Contributor IV

And the one before that? :smileyhappy: , where you set the DISTRO etc?

0 Kudos
Reply