Converter SMPTE 274 interface to MIPI CSI

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Converter SMPTE 274 interface to MIPI CSI

3,594 Views
dpuaaron
Contributor II

We have a custom whose camera is not MIPI CSI interface but SMPTE 274. Is there any IC chip or design scheme which can converter SMPTE 274 to MIPI CSI? Attachment is camera's brief introduction.

Labels (2)
0 Kudos
Reply
1 Reply

2,071 Views
igorpadykov
NXP Employee
NXP Employee

Hi Pu

according to document sensors have video digital output: Y/Cb/Cr 4:2:2 via LVDS

so it is necessary to use LVDS to MIPI CSI-2 converter like adv7782 or other.

SMPTE 274 describes used data format.


Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply