Hello,
Is it possible to control I2S/SAI controller from A7 domain in iMX7ULP?
By default, I2S/SAI drivers are available in M4 SDK (part of FreeRTOS) provided in the release package and are enabled by default to work with wm8960 codec. I could also see drivers available in linux (sound/soc/fsl/fsl_sai.c) and it is compatible with imx7ulp. So, can we control the I2S/SAI from A7 (Linux) itself ?
Thanks,
Jai Ganesh Sridharan
Solved! Go to Solution.
Hi Jai
seems sai0 is used for A7 :
imx7ulp-evk-wm8960.dts\dts\boot\arm\arch - linux-imx - i.MX Linux kernel
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Jai
seems sai0 is used for A7 :
imx7ulp-evk-wm8960.dts\dts\boot\arm\arch - linux-imx - i.MX Linux kernel
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Igor,
Thank you. I can see it is controlled by A7. Can I2C0 also be controlled from A7 itself ?
Thanks,
Jai Ganesh Sridharan
Hi Jai
seems this is possible configuring xrdc properly
(M4 SDK example ../driver_examples/xrdc/)
Best regards
igor