Controlling LVDS and backlight through Android App

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Controlling LVDS and backlight through Android App

2,514件の閲覧回数
hadarcadouri
Contributor I

Hello,

I'm working with an SBC which utilizes the iMX6 processor (Dual), running Android; where the app is in kiosk mode and has to be constantly on to communicate with the rest of the system.   I would like to define a power saving mode within the app itself, meaning that the app continues to communicate with the rest of the system, but controls the backlight, LVDS, and other hardware peripherals.

Is there a means by which the android app (not Linux command line) can enable/disable the LVDS and backlight outputs in real time?

thanks,

HC

ラベル(6)
0 件の賞賛
返信
2 返答(返信)

2,228件の閲覧回数
remioukrat
Contributor I

Hi,

You can modify backlight with Android API, like in this document :

Control Android's LCD backlight programmatically - TechRepublic

0 件の賞賛
返信

2,228件の閲覧回数
SergioSolis
NXP Employee
NXP Employee

Hadar,

were you able to modify the backlight with Remi's suggestion?, do you have any questions about it?

0 件の賞賛
返信