Control which displays QT application is output to

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Control which displays QT application is output to

1,373 Views
donjacobvellathottam
Contributor III

Hi,

I'm using an iMX8 processor and linux 5.15 built with yocto.

Currently I've managed to bring up two displays via LVDS and MIPI.

When I list the displays, it shows they are named XWAYLAND0 and XWAYLAND1. I've named them HDMI-A-1 and HDMI-A-2 in the weston.ini file.

I am able to execute two qt applications in two displays if I do that via the weston terminals inside the respective displays.

But can I control in which display the output of an application will be shown if I'm executing them via the debug terminal or using autoboot 

 

Thanks in advance

0 Kudos
Reply
2 Replies

1,338 Views
Zhiming_Liu
NXP TechSupport
NXP TechSupport

Hi
You may need select output in your QT application using QGuiApplication::screens.. etc.

Please refer QT api

https://doc.qt.io/qt-5/qguiapplication.html

Best Regards
Zhiming

0 Kudos
Reply

1,315 Views
donjacobvellathottam
Contributor III

Hi, thanks for the response

I was able to do it.

But is there any way to do it via the debug terminal (any cmd commands or anything)

I am trying to show a demo application, and I might need to send the output to either one of the screens. So, hard coding the display name into the application is not suitable now.

I'm trying to see if there are any commands that I can type in before executing the application to direct the output to a specific screen of choice.

I tried to use the 

DISPLAY=:

command but it didn't help

0 Kudos
Reply