Control Register configuration

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Control Register configuration

1,630 Views
dhanushvenugopa
Contributor I

Hi,

I am using the imx6ul evk board with yocto 4.9.x version ,since i need more number of gpio's I'm tring to mux the ethernet pins ,what value need to be set in the control register, so that the pin gets toggled with the voltage 0 and 3.3v when the  pin is made low and high respectively

Labels (1)
0 Kudos
Reply
1 Reply

1,547 Views
igorpadykov
NXP Employee
NXP Employee

Hi Dhanush

for i.MX6UL gpio control one can look at

Simple GPIO Example - quandry 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply