Contracted developer for iMX6SL needed (+some questions)

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Contracted developer for iMX6SL needed (+some questions)

2,090件の閲覧回数
ArtyomKamshilin
Contributor II

Hi all,

We have a few issues trying to set up the iMX6SL-EVK based development environment. Unless someone has a simple answer, we'd be willing to farm this out to someone who can solve this. Host environment is Ubuntu 12.04 LTS with all recent updates, LTIB (L3.0.35_12.10.02_ER_SOURCE) with all patches applied for successful compilation under 12.04.

Here are the issues:

1. When trying to use LTIB to compile libusb version 1.0.9, (the bundled 0.1.8 has problems), libtool is entering some kind of infinite loop, killing the host machine in under 10 seconds. It looks like some kind of a fork bomb. The same behavior has been observed on Ubuntu 10.04 LTS. Libusb 0.1.12 compilation fails with a "file not found" error (the same package was built OK on an older iMX28 LTIB).

2. Using "preconfig" setting in LTIB, and no extra packages, I end up with a Linux FS that only works correctly after the power switch has been turned ON - if I reset it using "reset" button, in 50% of cases kernel fails to load from TFTP, and USB devices fail to enumerate every second time or so (so libusb is not even kicking in yet). Flipping power switch off and back on solves until the next reset. Any ideas?

It's kind of crazy, and I need this to work soon. Thanks.

Regards,

Arty

ラベル(2)
0 件の賞賛
返信
3 返答(返信)

1,962件の閲覧回数
YixingKong
Senior Contributor IV

Artem

This discussion is closed since no activity. If you still need help, please feel free to reply with an update to this discussion, or create another discussion.

Thanks,

Yixing

0 件の賞賛
返信

1,962件の閲覧回数
YixingKong
Senior Contributor IV

Artem

We have not got your response yet and will close the discussion in 3 days. If you still need help, please feel free to

reply with an update to this discussion.
Thanks,
Yixing

0 件の賞賛
返信

1,962件の閲覧回数
YixingKong
Senior Contributor IV

Artem

We are sorry for getting back to you so late. Are you still stuck with the issue? If you have somehow

to resolved the issue, can we close the discussion? If you still need Freescale help, please feel free

to contact us.

Thanks,
Yixing

0 件の賞賛
返信